I'm using a UCD90160 to power up/down many rails. I want to make sure the sequencer goes through the right sequence, before I power up the rails for the first time. I included in the power supply design, a way to disable the power in to all rails, so I can observe the sequencing before the power is applied. Unfortunalely, this means that all of the monitors will not be getting voltages that are in tolerance. To get around this, I removed all rail dependancies, and did all the sequencing based on time only. The power-on delays look similar to the timing graph in Fusion Designer, but the power-off delays are not correct. Two rails that have quite different power-off delays are shutting off at the same time, and changing the delay values has no effect. I have attached the .xml file for this configuration. An help is appreciated. I'm in a bit of a bind on this one. Thanks.