This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2040

Other Parts Discussed in Thread: BQ2040

Hi ,

I am using the BQ2040 with a two cell Li-Ion battery. Recently we have had some problems with indication LEDs as they show incorrect information about the status of the cells:

The following are the read backs from the BQ2040:

Relative charge 65

Rem cap 3694mAh

Full cap 5664 mAh

Design cap 5200 mAh

Voltage 7547 mV

Abs charge 71

But we get only one LED when the \DISP is pulled low. Is there a explenation for this?

/BR