Hi
My coustomer want to use the TPS542951.
But coustomer don't need ch2
In this case below pin how to connect.
I already proposal TPS54227. But the coustomer want a same board that has a design previously.
This design can not EN2 is low. Because EN1 and EN2 is very near,,,
[1] VIN2:13V
[2] BST2:
[3] SW2:
[4] PGND:
[5] SS2:
[6] VFB2:
Best regards,
masa