I'm trying to work out a design with this part and I'm finding some shortcomings with it.
Why does this controller have a liberal 65ns forced dead time between the switch drivers. When running at 750kHz and 50% duty cycle it spends almost 25% of the pulse riding the body diode in the high side switch. With the high output currents I require it wastes a ton of power and creates heating issues.
The TPS43061 has a limited range on duty cycle. It forces pulse skipping under 10% and tops out at 75% with maximal switching frequency. Why would anyone design a boost controller than can not run in CCM down to zero duty cycle?
There's no pin option to force CCM. Why is that function not provided? It's better to let inductor current go negative and avoid pulse skipping if the power savings are not needed. Instead there's a "power good" pin. That's a redundant function since startup time is programmable.
Current mode is nice because it's easier to compensate, but why is maximal sense input only 60mV? A part with external switches is more suitable for a high output design. That calls for inductor DCR sensing which makes such a low sense limit harder to design around.
Normally TI parts offer superior performance and features. What happened with this one. Is this one they gave to the interns?
I'm going to work out a design using this part anyway since boost controllers like this one are not exactly a dime a dozen, but it's discouraging to see these shortcomings end up in my design. For a rather unique part such as this, I would have expected TI to put their usual high performance and liberal feature set into it.