Hi,
I am trying to figure out, with the least amount of components, an IC to use, that is able to operate from at least 1.6v/1.8v with up to 9v input and a regulated LDO output of preferably +/-6v or if not, then +/-5v.
Input would be a single supply voltage from either 2x NiCD/NiMH or a 1x/2x Li-Ion/Li-Pol batteries.
I remember coming across a buck/boost design with an inverter option in a single ic but I can not locate it.
It should be able to operate as low as 20 mAh / 40 mAh upto 400 mAh continuously.
Thank you.