This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS24720 Reverse Blocking Implementation

Other Parts Discussed in Thread: TPS24720, TPS24751, TPS24750

Hi there.

Is there any problem to implement reverse blocking with two back-to-back N-MOSFETS using TPS24720 , like in  TPS24751 hot-swap with internal and external MOSFET ? I need to consider an option to protect the system with more than 12A load as in TPS24751 , so the TPS24720  is a natural choice.

Thank you.