Hi,
I am planning to use the part LM1085IT-5.0 for generating 5V from a 14V supply, and the max load current is expected to be ~0.1A. I was specifically interested in the junction-to-ambient thermal resistance spec, and I'm planning to solder the tab of the TO-220 package to a metal area on the PCB.
In the specsheet, figure 21 is a graph named heat sink thermal resistance vs area. My doubt is, can I consider the quantity given on the Y axis of this graph, ie, "PCB heat sink thermal resistance(degC/W)" as the final junction-to-ambient thermal resistance or theta j-A? For instance, going by the graph, if I solder the tab of the T-220 package to metal filled area of area 5 sq cm, can you please tell if I can expect a theta j-A of ~25degC/W?
This aspect is important for my application as I will be doing some temperature testing on the board, and there are chances of the ambient temperature reaching ~80C. I'm more interested in using a linear regulator rather than a switching regulator for my application, so I wanted to confirm if this IC would be a good choice.
Thanks,
Anoop