Dear TI support,
I will do a multi cell balancing configuration (4s or 6S).
My charger will detect which battry is connected and set the configuration with MOSFETs that are controlled by a µcontroller.
But I have a problem because in the datasheet, it say that Cell-to-cell differential unused (here VC4 to VC1 for 4S or VC2 to VC1 for 6s) should be tied together and pull up to the most positive cell
(http://www.ti.com/lit/ds/symlink/bq77908a.pdf p36-37) but like that, if something goes wrong (wrong detection of the type of battery), some cell can be in short circuit (due to my MOSFETs controlled by the µcontroller).
My question is: Can I just pull up every unused cell to the most positive used cell without tied them together?
Regards.
Cédric