Hi, we are using TPS62091 in one of our designs, PFA schematic.
I need your help to select the appropriate Inductor.
The "Inductor Selection" topic in TPS62091 datasheet does not discuss about the Inductance. Instead it speaks only about the Saturation current and DC resistance of inductor. I have used 1uH inductor as recommended in the datamanual but have no understanding about it to justify the value of inductance(why 1uH and why not 470nH)?
Kindly help me in this regard. Other details are as mentioned below:
Vout = 3.3V fixed
Iout = 3.5A
Switching frequency = 2.8MHz (default)