Hello,
I'm asking for some help and or tips on a LM2678-ADJ current source conversion circuit. I have built the LM2678-ADJ voltage source on a breadboard and have it working but i'm trying to convert it into a adjustable current source to charge NiMH battery packs (24V 5Amp/Hour). I have added a few op-amps and made a somewhat working current source but it's unstable and there is a portion of the range that it jumps through. Currently the range is from ~50 mA to ~2 Amps but at ~660 mA it will jump straight to 2 Amps.
The attached .zip file contains images of both schematics. Schematic 1 is the voltage source and Schematic 2 is the current source version.
I don't understand why the current jumps any tips and/or opinions is greatly appreciated.
Thank you