This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

choosing LED driver

Other Parts Discussed in Thread: LM3466, UCC28810

 

There are number of driver ICs and lot of specs, bit difficult to choose the best one.  Can you help us to choose LED Driver.

                                                                          

Load is

 

7 Strings

Each string is 14 LEDs

So 14 LEDs in Series connection

And such 7 Strings are connected in parallel

Total Load – 50V / 420mA

 

The above arrangement is current arrangement. But flexibility exists to rework on Series Parallel Connection – final output load is 18W

 

LED Specs:

Voltage : 3.6V                          

Current: 60mA

Power: .2W

 

Input

We are having two models

  1. DC Voltage (Flexibility exists)
  2. 230VAC Mains

 

Final Product

General Lighting - Light Panel for Commercial application