This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53515 Inductor DCR

Other Parts Discussed in Thread: TPS53515

Hello,

Does the TPS53515 have a recommended or required maximum inductor DCR?

In my design (12V input, 3.3V output, 3A, 500MHz) I want use inductor IHLP2525CZER3R3M01 (Vishay) which has DCR of 28 mOhm .WEBENCH is recommends that inductor DCR was less than 15 mOhm. Can I use that inductor?

Regards,
Sergei