Hi,
I am new to battery management and so I have some naive questions:
I have a core System running at 3V3 and a cellphone module, which needs 3V3 and 3V7 for the cell phone transmitter part. Normally the System is powered by two car batteries in series (20V-30V) doing automatically measurements in the field. If the main supply Drops (no sun or fuel cell dry out and batteries pretty empty) the core should try to live for a while to send Status/ error messages and waiting for new energy. During this phase no measurement were taken.
==> I Need a battery management chip, taking 5V at the Input (USB Client to have a Interface for Service personal) and delivering 3V7 for the cell phone Transmitter and I will make 3V3 out of 3V7 using a linear LDO. A SMPS makes 5V out of 20V-30V as Long as this power source is available. If Service takes place, the Service guy can take the core and power it by USB from his Laptop or tablet using USB-OTG of his tablet. I dont Need USB-OTG at the measurement System.
Is the bq2426x such a chip? Or is there another chip recommended? My core can deal with UART, SPI, I²C, no Problem there where also GPIOs leftt if needed. The current dramw by my core isn't that high, all in all less than 1A. The cell phone/GPS/GLONASS module type isn't fixed at that time, so I can't give a certain value, sorry.
THANKS FOR HELPING A NEWBIE.
With best regards
Gerhard