Hola,
mi pregunta es si se puede utilizar la herramienta de desarrollo SM3320-BATT-EV/NOPB para en vez de cargar una bateria, usar a su salida un electroventilador en continua. Y tambien si la tension de salida se puede hacer variable de manera que pueda llegar a 24V usando el convertidor DC/DC.
Gracias---------------
Hello,
my question is whether you can use the development tool for SM3320-BATT-EV/NOPB instead of charging a battery, use an electric fan at its output continuously. And also if the output voltage can be made variable so it can reach 24V using the DC/DC converter.
thanks
my question is whether you can use the development tool for SM3320-BATT-EV/NOPB instead of charging a battery, use an electric fan at its output continuously. And also if the output voltage can be made variable so it can reach 24V using the DC/DC converter.
thanks