There are the following contents to the data sheet. (p.23)
"The following equations are used to determine if the minimum TON target of 300 ns and minimum TDMAG target of 1.1 μs is achieved."
Will these have the need to keep?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There are the following contents to the data sheet. (p.23)
"The following equations are used to determine if the minimum TON target of 300 ns and minimum TDMAG target of 1.1 μs is achieved."
Will these have the need to keep?
As a result of calculation : Ton(min) = 242ns
As a result of calculation : TDMAG(min) = 1.32us
Is there a problem?