Thank You.
Hi,
I'm using regulator TPS61040 to control the led backlight exactly as in figure 22 on page no 16 of the datasheet.
I've changed the Rs to 57R6, because I need I_LED = 20 mA, and I've fixed EN in 3,3V to test.
The problem is that when Vin changes, Vout changes too.
I've measured FB's voltage and it's changed too. To Vin = 5V => V_FB ~0,55V and to Vin = 3V => V_FB = 0,45V
I've understood that FB's Voltage would be fixed and equal 1,23V.
During my tests, I noted that if Vin <=2,2V, V_FB goes to 1,23V. (In this situation V_EN has been bigger than Vin)
I don't understand why this behavior.
In my aplication, I will work with 3,3V <= Vin <= 6V.
Can someone please help me?
Regards,
Conrado