Hi
Let me know the enable pin absolute maximum at TPS40170.
There is an output terminal Enable pin in P.3, but described as input pin in P.7.
Best regards,
masa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Let me know the enable pin absolute maximum at TPS40170.
There is an output terminal Enable pin in P.3, but described as input pin in P.7.
Best regards,
masa
The absolute maximum is 8.8V as listed in the table on P.3. The input and output listings are not very important in the absolute maximum table. For all pins if the voltage exceeds the rating due to an externally applied voltage or a condition which causes the IC to force the pin to reach the voltage listed there is risk of damaging the pin.
The ENABLE pin should technically be an input voltage but it seems it was kept with all other 8.8V rated pins in the table on P.3.