This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596-5 external components

Dear Yang, good morning!

Please, answer

I choose the elements for power supply. Webench offers the next components: output cap 150µF, 360 mOhm, input cap - 22 µF ceramic. Please, see attach.

QUESTIONS:

  1. Can I choose output cap 150 µF, 10V (tantalum) 700 mOhm? There is no 360 mOhm in the KEMET list. I need cap for minus 40 C temperature.
  2. Whether it is necessary to use input cap  22µF capacitor? May be I can use 2-3µF cap?
  3. Whether it makes sense to install C3 - 1 µF ?

        Dear, Yang, please inform your web service, that  forum E2E pages opens very bad - very large delay. And I often need to load a page multiple times in a row. 

TIA.

Sincerely,

Vladimir Naumenkov

www.agat.by

LM2596-5.RAR