This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5035C for Full-Bridge application

Guru 29720 points
Other Parts Discussed in Thread: LM5035C, LM5045
Hi Team,
 
My customer consider to use LM5035C(Half-Bridge Controller) for Full-Bridge application.
He thinks more cost effective than to use LM5045/46(Full-Bridge Controller).
 
My customer's board specification is the following.
---------------------------------------------
Input: 48V
Output: 12V / 33A(400W)
---------------------------------------------
Does TI has a track record for using LM5035C for Full-Bridge application?
My customer would like to confirm if TI has reference design for this case.
 
Best Regards,
Yaita / Japan disty