Hi,
I'm using the LMZ23608 for a 24V / 5V conversion on a new design, and I am experiencing some issues. I powered on the board, and after a while the 24V power supply indicates an overcurrent (current limited to 1.13A). I disconnected the power supply and measured a resistance of about 2 ohms between the 5V supply rail and ground. I unsoldered the LMZ23608 and the short-circuit was not there anymore. The problem happenned in two boards already, and it seems to happen randomly.
What are the reasons why the LMZ23608 would be short-circuited ? Overcurrent ? Overheating ? What about its overcurrent protection and thermal protection ? Today I don't know if the problem occurs because there is another problem on the LMZ23608 load, or if the problem is dued to the LMZ23608 itlself.
In normal operation, the cunsumption on the 5V rail is 800mA, and the case temperature of the LMZ23608 is about 60°C, nothing that seems to exceed its spectication.
Thank you for your help.