I have configured the TPS2511 to limit current at 500mA (min). If a device is plugged in that has a very low battery, it will assume that I can supply more than the 500mA since it negotiates as a DCP. The problem is that the voltage drops across the FET enough to trigger a device shutdown. This will loop when the devices turns back on.
I also read in the TI forum that
http://e2e.ti.com/support/power_management/power_interface/f/204/t/240121.aspx
So, I am now looking at the TPS2546 now so I can force the SDP mode. However, the datasheet states:
Standard Downstream Port (SDP) USB 2.0/USB 3.0
An SDP is a traditional USB port that follows USB 2.0/3.0 protocol and supplies a minimum of 500mA/900mA per
port. USB 2.0/3.0 communications is supported, and the host controller must be active to allow charging.
I don’t have a host controller since this is just like a wall charger. Do you think this configuration would still allow charging?
Calum