This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About LM3432 when little number of the LED series (Low VLED : 12V).

Guru 19655 points


When client use VLED and LM3432_Vin in 12V, they will not use step-up DC/DC such as LM3430.
(Constitute it only in LM3432)
is these idea no problem?

Best regards,

Satoshi

  • Sorry,  I had find mistake of VLED.

    Please refer to below, correction of a mistake, and additional information.

    ------------------------------------------

    ・VLED:30V (12V is mistake)

    ・LM3432 Vin is 12V

    ・Number of LED:9 series, 4 parallel

    ・IF:20mA / 1 line

    ------------------------------------------

    Best regards,

    Satoshi

     

  • As for the content on which it questioned the other day, how about the situation?

    Please teach if there are specs and information necessary to answer.

    I will confirm it.