I am using the LM2621 to boost 1.8v-3v input to 7v output. The datasheet says Vdd must be 2.5v-5v.
Most implementations I have seen online just power Vdd through a 500ohm resistor from Vout (and the Boot pin directly from Vout), even if Vout is above 5v, and nobody has reported a problem. I am using it that way in my prototype (and it's okay so far), because the datasheet suggested method did not work .
In the Bootstrapping section, the datasheet says when Vout is over 5v, VDD can be connected to Vout stepped down using a linear regulator. Can you suggest a regulator that would work? I used an LDO, but it did NOT work. The DC-DC could never even get started, because as it raised Vout, that did NOT go through the LDO to get back to Vdd, so the bootstrapping didn't work. The 3.3v LDO I chose, the output stayed at 0v because its input, Vout, never got high enough. And Vout never got high enough because Vdd was never there. Both waiting for the other.
So, two questions:
1. Is it OK to run Vdd from 7v through a 500 ohm resistor, just as it is done from 5v? According to the datasheet, it won't damage anything, but will the circuit no longer function within specs? Which specs? Datasheet says:
Absolute maximum ratings indicate limits beyond which damage to the device may occur. Electrical specifications do not apply when operating the device outside of its rated operating conditions.
The absolute max for Vdd is 10v. The operating conditions ar 2.5v-5v.
2. Please suggest a simple inexpensive "linear regulator" that will work (as suggested in the datasheet Bootstrapping section) - one that will pass enough voltage and current through it during startup to allow startup to occur -- Vout is connected to BOOT and to the LDO input, LDO output going back to Vdd.
Thank you.
Jay