Hi
Could you tell me the minimum duty cycle at the LMR62421?
Best regards,
masa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Could you tell me the minimum duty cycle at the LMR62421?
Best regards,
masa
I will try to contact a product engineer to see if he has any data on what min and max from characterization were.
Marc
I talked with the product engineer and he has no data on the min and max of the minimum duty cycle. It was only tested as a typical for the datasheet.
Regards,
Marc
Hi
Thank you for your reply!
I discussed with my customer.
Coustomer very need this parameter.
Because of they spec is below.
Vin:3.3V
Inductor input voltage:14V
(Its mean separate Vin and inductor input voltage)
Vout:15V
Iout:500mA
customer consider that min duty cycle(maximum min duty cycle spec).
So could you tell me design spec.
Best regards,
masa