hi im using tlc61220 for driving a led of 3.2v/120mA.
In this i connected as u suggested in data sheet
r1=1M ohm,r2=180k ohm,with 4.7 uH.
can u suggest the resistor values to drive as 3.3v/120mA.
thanking you,
naidu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
what i meant is the resistors as u mentioned in datasheet i.e., Vout to FB & FB TO GND.(r1 &r2)
I want to know the changes to drive 3.2v/120mA
my input voltage is 1.2V to 2.8V
what i have to do for changing the output cerrent .
Either it can be change the capacitors or resistors(i/p or o/p)
thanking you
naidu
TLV61220 can't drive 3.3V/120mA from 1.2V input.and i would suggest TPS61020.
if possible, apply an EVM to evaluate the performance before design your project.
jasper li
maybe Vin=3.1...... i don't suggest to use this device to support 120mA output current.
Boost Converter Solution
jasper li
Please refer to the figure 1, 2 in the datasheet page 6 for the maximum output current. thanks
jasper li