This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCP022415D Peak current

I need a power supply to deliver a 2.5W pulse to an offboard load.  The load is switched for 50mS with a maximum duty cycle of 5%.  Typical duty cycle is <1%.  I like the isolation, and I don't think output regulation should be an issue.

The duty cycle is low enough where I don't think heat should be an issue.  Would the DCP021212 be able to handle this peak current?    If not, would this be possible with a fairly large output cap connected?