This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5008MM/NOPB - continuous conduction vs discontinuous conduction

Good morning, I am trying to get a better understanding of this converter and I am hoping you may be able to provide me with some insight. 

My first question is in regards to the voltage requirements for the chip.  We have a circuit where this part is used, and the output of the step down regulator is sized to provide 12 V out.  Given that the chip is a step down regulator (as opposed to a step up), my interpretation is that the input voltage would need a minimum of 12V at the input.  Is this correct?  ...The reason I ask is that we are seeing the chip function down to 9 volts and I was wondering if powering the chip this low would stress the chip?  If I set my output to be 12V, is there a minimum input voltage that I should provide?

My goal is to get a better understanding of the chip, as the engineer who designed the circuit set the minimum input voltage as 30V, and I have a customer that would like to power it below 30V (possibly down to 12V).  I am trying to understand the chip better to determine why the engineer set the min input voltage at 30V.  I recognize that there is likely a very good reason why the floor was set to 30V, but I need to understand the part better in order to provide a rationale explanation as to why or why not the chip can be powered below 30V.  *The input voltage comes directly from an input power supply and only connects to this chip (not any other parts)

I also have further question in regards to the ripple voltage and the continuous conduction vs. discontinuous conduction modes of operation, but I will hold those questions for now until we get a dialogue started.

Thank you in advance for your help in understanding this part better.

Thanks,

Steve