Other Parts Discussed in Thread: BQ24032A, TPS63010
I have a board where the output of a bq20403x part feeds a buck/boost regulator. When increase the load on the regulator to the point it can no longer regulate the output voltage of the regulator of course crashes but this also triggers the bq2403x part to enter DPPM mode. The problem is I never come out of DPPM mode and the output of the bq2403x gets stuck at around 1.8V. I don't have a microcontroller or any logic to connect to the DPPM pin to reset the part so I have to do a power reset to recover. So far I've tried increasing the capacitance on the DPPM pin to the datasheet maximum recommended of 10nF to delay the onset of the DPPM mode and I've tried lowering the resistor on the DPPM pin to lower the voltage at which DPPM is triggered but neither seem to be having an effect. I think I must be missing somthing here but I can't seem to figure it out and was wondering if someone could help me out. So far the only thing I've tried that has worked is connecting the DPPM pin to ground so that the part doesn't enter DPPM mode but this isn't recommended. I'd be happy to give further expanation about any other details if it somehow helps. Thanks.