I'm looking for a simple solution to convert 3.3V to 2.5V with EN input. It is required that the output should be within the duration when EN is '1'. LM3671 seems to be a choice, but I'm not sure if such timing requirement can be satisfied because the datasheet shows start up timing only. Can anyone provide details about shutting down? Thanks.