LM2990 Negative LDO - output oscillation question
What we are seeing is ~1Vpp @ ~26KHZ oscillation at the LM2990 output.
When we remove Cout the oscillation persists, but with a different frequency.
Cin and Cout are 4.7uF X7R 25V ceramic caps.
When we replace Cout with a 10uF 10V 3.50Ω tantalum the oscillation stops.
We are confused because the ceramic cap has a lower ESR (<1Ohm ) than the tantalum (2.5Ohm). Shouldn’t the lower ESR part work fine? The customer is trying to get away from using tantalums due to their poor reliability.
Also, We would like to verify that the LM2990 has a maximum ESR of 10Ω for its output cap and not a minimum.