This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS75003 IC not working properly

Other Parts Discussed in Thread: TPS75003

Hello,

I am currently using TPS75003 IC in one of my designs using. SPARTAN 3 FPGA.  The schematic is attached.

Iam not seeing any switching waveforms at the gate of either Q2 or Q1. I am seeing a continuous DC voltage at gate of the transistors( i.e; no switching is happening). But the LDO output (2.5V) is fine.

The values of the passives, MOSFET and diodes are as per the refernce schematic given in the IC datasheet. The observed dc-dc converter output voltages are Vin- MOSFET drop. The continuity between the IC pins and the circuit components as been checked and are found to be OK. 6266.8311.tps75003.pdf

On a different PCB, I assembled the components required for, only the 1.2V section. Still the behaviour observed is same.

Kindly suggest future action to be taken.

Regards, Vikram.R