This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bq27510 Golden Image Programming over firmware

Other Parts Discussed in Thread: BQ27510

Hello,

if I have created a golden image.dfi file explained like in slua544.pdf it´s possible to write this file into flash without connecting with extern tools like bq Evaluation Software? I will to do this like the way I explain now.

  1. In production I can write the .dfi file into flash of thy Microcontroller.
  2. If firmware starts there is a production modus and now I write to the Bq27510 flash e.g.
    1. first I send unsealed key
    2. then I jump to the configuration subclass ID 48
    3. I can change the design capacity (I already do this)
  3. Then I will copy .dfi file from µC flash and send this to the Bq27510 with th I2C interface.
  4. Afterwards I delete .dfi file in µC flash

Now my questions to you.

Is this a possible solution or must the golden image file write to dataflash every time with external connection? Which command must be set before sending .dfi file to the Bq27510? Like CAL_MODE 0x0040? How large is the golden image file? I have found examples of 2kB size.

For us this would be a comfortable way to make the production of our device very easily.

Thank you for you answers


Best Regards

Eckart