This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to calculate the soft start time of TPS54427 with large capacitive load

Hi,

           The load requires a large input capacitance, so the capacitance is CD19 and CD20 in the below SCH. The total is 940uF. How to calculate the soft start time so I can choose the proper SS capacitor? I found if I set the SS capacitor as 10nF, sometimes, it didn't power up properly, but 20nF is fine.

           Thanks.

 

  • Can you post waveforms of the good and bad start up?  I would need to see the SW node and inductor current as well as the SS and Vout voltages.  Your output filter is not within the recommended values for proper operation.  Can you tell me the ESR of CD19?  With that output filter, the IC may not work as intended.