I'm using a LM22672 to step down 24V to 5V. Occasionally (1 time in 200-300) the LM22672 will come up stuck in a limit mode at about 2.2 V with 140ns wide pulses. It will stay in this mode until power is cycled.
This is a related problem to an earlier discussion (LM22672 into ideal diode weird behavior). The suggested solution of adding a reversed bias schotky diode from output to imput seems to improve how often the problem occurs, but doesn't eliminate it. What I am seeing now is that the LM22672 can enter the limit state without the other supply being present.
The 24 V power supply doesn't always behave nicely. It can be hot connected and there can be a lot of contact bounce when first connected. This can last up to ~100 ms. However I have found no correlation between the contact chatter and the LM22672 going into the limit state. Or for that matter between anything & having it go into the limit state.
Can a similar latchup occur with other pins (besides Vout) being higher than Vin? The soft start and the sync pins are possible candidates since they could be at higher voltages then Vin during the input transients.