Hello
I bought a evaluation board TPS62130-505, the output voltage is 3.3 and the datasheet suggest the maximum output current is 3A, but when I program my dc electronic load to 3A, the output voltage was 3.3, but I want to know what is the current limit , I forced the evaluation board to deliver until 3.9A, when the electronic load did consume 4A, the output voltage did fall down quickly, then the limit is 3.9A, is recommend to do that?, what happen If the electronic load consumes more that 3A?