This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

External MOSFETER SELECTION OF MC33063A

Other Parts Discussed in Thread: MC33063A

Hi All,

I just used MC33063A in my power system which one is a step-down regulator. And I would like to use an external MOSFET to enhance the current value.  The NPN switch is simple on control but there is a potential risk on Vgs due to the maximal 40V input voltage (normally the Vgs < 20V). For PNP switch the control is complex than NPN switch. Lower division resistance is good for switch speed but with higher power consumption. Higher division resistance is beneficial on power consumption but bad on switch speed.  How can i deal with it? Please give you adviance on this. Below is the conditions of regulator.

 1. Input voltage: 40V

 2. Output is 5V @ 1A

 3. The minimal heating generation

Thanks in advanced!

Best Regard

Kurt Wu