Dear TI,
I'm are trying to desing a switching circuit to regulate hight impedance r/c source. i tried with LM2596adj to achieve 6v with 130ma load but it failed because of heavy current startup load. I presume that I need to implement soft start circuit or to change the chip for some other with adjustable soft start. Can you advice additional soft start circuit for LM2596adj or if it's not possible to suggest replacement chip (40v input max load 300ma) with minimum of 0.5sec soft start?