Hi,
I'm having facing a serious issue with the TPS65950 RTC module interfaced with the OMAP3530 processor.
Code is done for the low level driver to check the rtc functionality.
W're using the i2c interface in the processor side. The RTC module is enabled in the control register but still the rtc is not running.
When polling for the status register and seen the rtc module is still saying rtc is frozen.
Please help , tell me what the steps need to be done.
I cross checked with the linux rtc code also . the exact same values are configured in my low level driver.
Regards,
Devakumar