Hi
I have an unusual issue with my setup. It uses a 5V/1A wall wart as the power source.
For 2 NiCD batteries in series this setup has been working fine but recently I needed to charge 4 NiMH batteries in series (1.2V AA type) ive had the LED indicator light up the moment the cells were connected (while the setup was not connected to the 5V 1A wall wart) suggesting a reverse current flow.
The switching mosfet was checked and its not shorted so I presume its probably the internal mosfet diode. Im using a TSM3457, which has similar specs to Si3455 and a Vds of -30V.
Would a series diode on the power rail between the BQ2000 VCC and the mosfet source pin be enough or is it a symptom of something else ?
Regards
Soumitra