When TPS54060 is used by Inverting output, does Enable become a negative voltage input?
I seems to be inverted if Fig14 of the following application notes is seen. http://www.tij.co.jp/jp/lit/an/slva317b/slva317b.pdf
Request spec are Vin:24V/Vout:-16.8V/Iout:100mA.
Client uses with two or more TPS54040A, and they want to control by one Enable signal.
Best regards,
Satoshi