Hi all,
I am working on a design using OMAP3530 and TPS65930.
System has to be powered from 2-Cell Li-Ion battery (max 8.4V) or 12V DC wall supply and TPS65930 provides the main power rails to the board and has a maximum limit of
4.7V on its VBAT input and a nominal of 4.2V (minimal 3.3V).
To meet TPS65930 requirement there need to be used DC-DC regulator to convert those input voltages in range about 5-12V to 4.2V. I will use Switching DC-DC Buck Converter.
Final device need to operate in following modes:
1 On/ Full Active,
2 Hibernate/Deep sleep mode,
3 Power Off mode,
Power Off mode I understand as VBAT=0V for TPS65930 and 4.2V Dc/Dc Converter is OFF. That will be something like battery removal emulation.
My question is:
Q: Is there any possibility to turn off DC-DC Buck Converter using OMAP / TPS65930 Signals (sys_off_mode/nSLEEP, SYSEN, REGEN, GPIO...) or additional logic under Omap control?
Thanks,
Bartek Swierczek