Hi,
I am designing a DC-DC converter with the following spec's:
Vin (V) : 44 to 65 V
Vout(V) : 24V
Iout : 5 amp
I am planning to use LM5116 for the same. Can you please suggest me any better IC as well as important points to take into consideration while designing such applications.
This design is basically used in solar applications. Input from solar panel to be given to the solar inverter
Regards,
Rohan