This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ3060 communication wakeup issue when in sleep and under CUV state

Other Parts Discussed in Thread: BQ3060

Any reason why the SMbus communication  is not available  when the BQ3060 detects the CUV (DFET is OFF) state, and it goes into sleep state (since the sleep bit is ON) and cannot wake up via SMBus activity alone. Also BQ3060 has the broadcast bit set? cfg A is 0x0329, cfg B is  0x0C49, cfg C is 0x0002.  Definitely above the  threshold set for the shutdown of IC (7V) .

Pack does wake up on applying the charge voltage to the pack+/-, but curious why the SMBus is OFF.?