Other Parts Discussed in Thread: UC2906, UC3906
Hello everyone. I have built a circuit to charge a 24V/5Ah lead acid battery using UC2906. Although the datasheet is not very helpful/detailed, I tried to follow the instructions and get this working. But when the UC2906 gets in bulk charge state, the transistor is getting almost burnt... Probably something is wrong with my circuit, and that's what I ask for help to resolve. Here is the schematic:
A few data:
Configuration of the UC2906: DUAL STEP CURRENT CHARGER
Vbuck charge=24,6V
Vfloat=27,4V
Vholding current=27,6V
Ibuck charge=500mA
Iholding current=15mA
Vsupply=35Vdc