Hello,
I am considering using a LMZ30602 with an Artix 7 FPGA. It provides for power sequencing and has the shielded inductor and other qualities I want. I would be used for a 1V, 1.8V and 3.3V supply (all at less than 2A) converting power from 5 V.
When I run WEBENCH for an Artix 7, the LMZ30602 never is one of the alternatives. Is there a compatibility issue with the LMZ30602 and the Artix device that prevents WEBENCH from selecting this part?
Thanks for you help
Rob Curtis