I simulated LM3481-Q1 by the following conditions.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ryuji,
Yes, please go with at least 470nF on the Vcc cap. I will get this fixed in WEBENCH promptly.
The datasheet inductor values are picked to be in CCM at full load.
WEBENCH values actually use a different set of criteria. When using uncoupled inductors an instablility can occur at some operating points as ringing across the SEPIC capacitor that you don't see when using coupled inductors. You can get rid of this with a RC damping branch across the Cap, or there is a stability criteria in inductor selection that makes it so that this doesn't happen. WEBENCH uses this to do its inductor selection. (an simplification of the criteria is that L2 should be at least double L1)
The WEBENCH compensation is then designed for the power stage components it has selected. I would stick with the WEBENCH selected powerstage in this case.
Best regards,
Tommy