I am considering LM25088 for a design where an 18-36 V input voltage will be converted to an adjustable voltage between 2 V and 15 V (using current injection into the FB node to set the desired output voltage). The load will be between 0 mA and 2 A.
After reading the datasheet and doing some simulations in Tina TI, I am not at all sure that LM25088 will handle no load/light load well. I cannot find anything in the datasheet about pulse skipping or other means of maintaining regulation when there is little or no load and the simulation (a modified version of http://www.ti.com/lit/tsc/snvm567 with 10 kohm as the load and 500 ohms as R7) indicates that the output and feedback nodes rise far above the desired regulation point.
Can LM25088 be used when there might not be any load current?
Does it have pulse skipping built in?
Is there any other part that would be more suitable for this application?