Hi
I have a part of my circuit that use 2.8V for this I am planing to use LP5907. the problem is that it takes the part of circuit that provides the voltage to the LDO input some time until the voltage stabilize around 3V. it can even get to 15V before stabilizing on 3V.
is there a solution that can be applied here so I wont burn the LDO?
maybe some kind of switch that closes under certain voltage or something like that?
what is the name of such component so I will look for it in the site?
Regards,