Our customer has questions about UCC28701.
I'm posting the questions for a customer:
++++++++++++++++++++++++++++++++++++++++++++++
They observed the current of the DRV terminal of UCC28701.
The peak sink current:IDRV(peak) was 158mA(max) on their board.
The datasheet mentions "Continuous gate current sink: 50mA(max)"
(ABSOLUTE MAXIMUM RATINGS).
But no mention of "Peak gate current sink" in the datasheet.
1)Is the peak:158mA(max) OK?
2)How much is the value permitted of "Peak gate current sink" for UCC28701 ?
++++++++++++++++++++++++++++++++++++++++++++++
Thanks in advance.
Best regards,
Takishin