This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help me to find the right design for DC/DC converter with I/P range 70V to 150 V

I need a help to find the right design for the DC-Dc converter (Buck ) .
converter should operate from 70 V to 150 V input range . and the output is 15V /4A
i could not find the design more than 100V .
so please suggest me some design on the same.